cancel
Showing results for 
Search instead for 
Did you mean: 

High Speed Isochronous mode bInterval other than 1 not work

Daniel Squires
Associate II
Posted on November 03, 2016 at 14:02

Hi - I am trying to implement UAC 2  as part of a project. I  have setup the descriptors and it enumerates and is recognosed by the PC. The problem arisises when I try to stream the audio data to the PC. If I set the bInterval for the endpoint to anything other than 1 (125uS) the PC receives 0 length packets. It works set to 1 but sending such small packets so frequently is a very inieficent use of bus bandwidth.

Anybody have any ideas?

Edit : I should have mentioned that the Data_In callback never gets called with bInterval of more than 1 so the initial USBD_LL_Transmit  in the init function works and then no further calls. The PC ends sees response of success with length 0.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Daniel Squires
Associate II
Posted on January 19, 2017 at 13:49

I am seeing this with OUT endpoints now too.

I wonder if it relates to the fact that if you search for bInterval on google the first thing that comes up is 

http://www.beyondlogic.org/usbnutshell/usb5.shtml

 

which states :

6 bInterval 1 Number

Interval for polling endpoint data transfers. Value in frame counts. Ignored for Bulk & Control Endpoints. Isochronous must equal 1 and field may range from 1 to 255 for interrupt endpoints.

Which is incorrect according to page 47 of the USB2 standard which states :

An isochronous endpoint must specify its required bus access period. Full-/high-speed endpoints must

specify a desired period as (2

bInterval-1

) x F, where bInterval is in the range one to (and including) 16 and F is

125 μs for high-speed and 1ms for full-speed. This allows full-/high-speed isochronous transfers to have

rates slower than one transaction per (micro)frame. However, an isochronous endpoint must be prepared to

handle poll rates faster than the one specified. A host must not issue more than 1 transaction in a

(micro)frame for an isochronous endpoint unless the endpoint is high-speed, high-bandwidth (see below).

An isochronous IN endpoint must return a zero-length packet whenever data is requested at a faster interval

than the specified interval and data is not available.