cancel
Showing results for 
Search instead for 
Did you mean: 

Hi All I needed an urgent help on Timer Interrupt. Thanksc STM32F407VG

ncolincoli
Associate II
Posted on September 21, 2013 at 03:40

Hi all I have a project (@my uni) due in late November and i am really stretching all possible time to see something going.

Could Someone please help me as to why this below code ISR only happens once?

Thus the Orange LED on  Pin 13 flashes One tenth of a sec but the Blue one on Pin 15 which is meant to be flashing every sec isn't (ie: Stay on) i have been carefully following the code and the problem seems to be in the ISR itself, ie: it only happens once even though

(

TIM2->

EGR

|= TIM_EGR_UG

) is meant to be updating the flag every time the Counter reaches ARR value. I really don't seems to see why it isn't working can someone help me?

Many Thanks again

Regards

Entropy

/*

Timer ISR running on  STM32F407VG with COIDE

Please ignore the comments were meant for other development code. Thanks

*/

#include<stdint.h>

#include<stdlib.h>

#include <stdbool.h>

#include''stm32f4xx.h''

#include''stm32f4xx_rcc.h''

#include''stm32f4xx_tim.h''

#include''stm32f4xx_gpio.h''

#include''core_cm4.h''

 

volatile bool Process_Task = false;

 

void _delay_us(uint32_t us);

void _delay_ms(uint32_t ms);

void

TIM2_IRQHandler(

void

);

int main()

{

SystemInit();

 

GPIO_InitTypeDef

GPIO_InitStructure; GPIO_InitStructure;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD,

ENABLE

);

 RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3,

ENABLE

);

GPIO_InitStructure.

GPIO_Pin

= GPIO_Pin_12 | GPIO_Pin_13| GPIO_Pin_14| GPIO_Pin_15;

 GPIO_InitStructure.

GPIO_Mode

=

GPIO_Mode_OUT

;

 GPIO_InitStructure.

GPIO_OType

=

GPIO_OType_PP

;

GPIO_InitStructure.

GPIO_Speed

=

GPIO_Speed_100MHz

;

 GPIO_InitStructure.

GPIO_PuPd

=

GPIO_PuPd_NOPULL

;

 GPIO_Init(GPIOD, &GPIO_InitStructure);

NVIC_InitTypeDef

NVIC_InitStructure;

/* Enable the TIM2

gloabal

Interrupt */  NVIC_InitStructure.

NVIC_IRQChannel

=

TIM2_IRQn

;

NVIC_InitStructure.

NVIC_IRQChannelPreemptionPriority

= 0;

 NVIC_InitStructure.

NVIC_IRQChannelSubPriority

= 1;

NVIC_InitStructure.

NVIC_IRQChannelCmd

=

ENABLE

;

 NVIC_Init(&NVIC_InitStructure);

/* TIM2 clock enable */

TIM2->

PSC

= 41999;

 TIM2->

ARR

= 3999;

 TIM2->

CNT

= 0;

 TIM2->

EGR

|= TIM_EGR_UG;

 TIM2->

SR

&= ~ TIM_SR_UIF;

TIM2->

CR1

|= (TIM_CR1_OPM);

// Clear the update flag

TIM2->

DIER

|= TIM_DIER_UIE;

// Enable interrupt on update event

NVIC_EnableIRQ(

TIM2_IRQn

);

// Enable TIM6 IRQ

TIM2->

CR1

|= TIM_CR1_CEN; // Enable TIM6 counter

//while (!(TIM2->SR & TIM_SR_UIF));

 

while

(1)

{

GPIOD->

ODR

^= 1<<13;

_delay_ms(100);

}

}

void

TIM2_IRQHandler(

void

)

 {

if

(TIM2->

SR

& (TIM_SR_UIF)) 

 

// If update flag is set

 

{ {

GPIOD->

ODR

^= 1<<15; TIM2->

SR

&= ~TIM_SR_UIF;

 //Clear it.

//Process_Task = true; // Set D15 high

 // GPIOD->ODR |= 1<<15; // Interrupt has been handled

//_delay_ms(15);

 }

//delay_ms(15);

}

void _delay_us(uint32_t us)

{

TIM3->

PSC

= 83 ;

 

 

TIM3->

ARR

= us -1

TIM3->

CNT

= 0;

TIM3->

EGR

|= TIM_EGR_UG;

TIM3->

SR

&= ~ TIM_SR_UIF;

TIM3->

CR1

|= (TIM_CR1_OPM);

// Clear the update flag

TIM3->

CR1

|= TIM_CR1_CEN;

while

(!(TIM3->

SR

& TIM_SR_UIF));

}

void _delay_ms(uint32_t ms)

{

while

( ms -- > 0) {

_delay_us(1000);

}

}

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on September 30, 2013 at 15:20

And what's that testing? Presumably a cheap way to test if a singular high order bit is high or low. Just test the bit directly.

The connectivity in both cases is not sufficiently clearly stated to make much of a determination.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..