cancel
Showing results for 
Search instead for 
Did you mean: 

Help: Step-by-step guide to establish UDP communication with static IP using NetX Duo (via IOC) nucleo-n657x0-q

AlonSade
Visitor

Hello everyone,

I’m currently working on setting up UDP communication using NetX Duo with a static IP address, configured through STM32CubeMX (IOC) in nucleo n657x0-q.
Please note that the UDP communication needs to be initialized and executed in the Application (APPLI)not in the FSBL.

I’ve gone through several related threads in the community, but I still haven’t managed to get the communication working properly.

Could someone please provide a clear, step-by-step explanation or example of how to configure and initialize UDP communication (client or server) with a static IP in NetX Duo under APPLI?

I would greatly appreciate details on:

  • The correct IOC configuration (Ethernet, NetX Duo, IP, UDP, MPU etc.)

  • The proper initialization sequence in APPLI (how and when to start the network and socket)

  • Relevant NetX Duo API functions (e.g., nx_udp_socket_create, nx_udp_socket_bind, nx_udp_socket_send, nx_udp_socket_receive)

  • Common issues or pitfalls when moving UDP handling from FSBL to APPLI

Thank you in advance for your support and guidance!

Best regards,

Alon Sade

0 REPLIES 0