cancel
Showing results for 
Search instead for 
Did you mean: 

Help ! (First time with STM32)

Giuseppe Cipriano
Associate
Posted on March 09, 2018 at 18:17

Hi, i'm making some board with a STM32F042F6P6. Today i solder the board, i connected it with the USB cable but windows doesn't see it. Where am I wrong? Do i need to buy a ST-Link V2 Programmer? 

how do I connect it to the pins for the st link?

Thanks.. and sorry for bad english (google translate) and sorry again for the ignorance, it is the first time I use these STM.

This is the board 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on March 10, 2018 at 20:48

Without code the USB will do nothing. Not sure if specific part supports USB and DfuSe in system loader. Would need to pull BOOT0 high to get into loader at startup. Loader should always support USART connectivity mode, where you'd use FLASH Loader Demonstrator. 

For most any development you'd want a debugger pod like a ST-LINK, J-Link, etc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4
Posted on March 10, 2018 at 20:48

Without code the USB will do nothing. Not sure if specific part supports USB and DfuSe in system loader. Would need to pull BOOT0 high to get into loader at startup. Loader should always support USART connectivity mode, where you'd use FLASH Loader Demonstrator. 

For most any development you'd want a debugger pod like a ST-LINK, J-Link, etc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
Posted on March 11, 2018 at 10:41

First time with STM32

Do you have any experience with other microcontroller(s)? With programming in general?

For basic getting-started tips, see:

https://community.st.com/0D50X00009XkWm7SAF

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Giuseppe Cipriano
Associate
Posted on March 13, 2018 at 18:06

Hi thanks to all

A friend helped me, i soldered bad the usb connector
Posted on March 13, 2018 at 20:22

So please mark your question as 'solved'.

https://community.st.com/0D50X00009XkXxjSAF

 
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.