cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am Firmware engineer working on STM32G07 series board. While working with Flash memory I have unprotected Flash from Read and Write using STlinkUtility v 4.5.0, after this I am not able to Erase the Flash and hence not able to Debug and load.

SDesh.1
Associate II

Hello I am Firmware engineer working on STM32G07 series board. While working with Flash memory I have unprotected Flash from Read and Write using STlinkUtility v 4.5.0, after this I am not able to Erase the Flash and hence not able to Debug and load as STM32 CubeIDe internally gives Erase command to clear Flash and Writes the new code on to board, Kindly suggest how can i fix this. see attached image for details.

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Antoine Odonne
ST Employee

then regress to Level 0 :)

SDesh.1
Associate II

Thanks Antoine,

It worked :) Thanks for your suggestions.

Regards,

Shiv

Hello @SDesh.1​,

Try to use STM32Cube programmer, you can refer to the STM32CubeProgrammer v2.7.0 release information and you will find that release support the STM32G0, it's recommended to use Cube programmer instead of ST-Link utility

Mohamed Aymen