cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_UART_Transmit_DMA

Nandy K
Associate II
Posted on October 21, 2015 at 19:20

Hi,

I am using STM32F746.

It is connected with ST wifi module(SPWF01SC) via UART.

/* Buffer used for transmission */

uint8_t aTxBuffer[] = ''AT+S.SOCKD=8825\r\n'';

/* Buffer used for reception */

uint8_t aRxBuffer[RXBUFFERSIZE];

In the program I am using HAL_UART_Transmit_DMA to transfer  and HAL_UART_Receive_DMA to receive.

I am transmitting the buffer to start the wifi module and it is working fine.

Now I am sending a string ''PIP'' from my wifi module.

whenever I receive this string''PIP'' the MCU need to transmit back ''CIAO''.

In my case I am receiving the string CIAO only when I reset the MCU and also it is working fine only for the first time after reset then for the second time i need to send the string twice then i get the response but after that there is no response.

my main loop code :

  UartHandle.Instance        = USARTx;

  UartHandle.Init.BaudRate   = 115200;

  UartHandle.Init.WordLength = UART_WORDLENGTH_8B;

  UartHandle.Init.StopBits   = UART_STOPBITS_1;

  UartHandle.Init.Parity     = UART_PARITY_NONE;

  UartHandle.Init.HwFlowCtl  = UART_HWCONTROL_NONE;

  UartHandle.Init.Mode       = UART_MODE_TX_RX;

  if(HAL_UART_DeInit(&UartHandle) != HAL_OK)

  {

    Error_Handler();

  }  

  if(HAL_UART_Init(&UartHandle) != HAL_OK)

  {

    Error_Handler();

  }

   if(HAL_UART_Transmit_DMA(&UartHandle, (uint8_t*)aTxBuffer, TXBUFFERSIZE)!= HAL_OK)

  {

    Error_Handler();

  }

  

 /*##-3- Wait for the end of the transfer ###################################*/  

  while (UartReady != SET)

  {

  }

 while (1)

  {

      HAL_Delay(100);

    

      if(HAL_UART_Receive_DMA(&UartHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK)

      {

         // Error_Handler();

      }

     

      if(aRxBuffer[0]=='P'&&aRxBuffer[1]=='I'&&aRxBuffer[2]=='P')

      {

          aTxBuffer[0]='C';

          aTxBuffer[1]='I';

          aTxBuffer[2]='A';

          aTxBuffer[3]='O';

          aTxBuffer[4]='\r';

          aTxBuffer[5]='\n';

          

           BSP_LED_On(LED1); 

          txBuf = 5;

        if(HAL_UART_DeInit(&UartHandle) != HAL_OK)

        {

          Error_Handler();

        }  

        if(HAL_UART_Init(&UartHandle) != HAL_OK)

        {

          Error_Handler();

        }

        if(HAL_UART_Transmit_DMA(&UartHandle, (uint8_t*)aTxBuffer, txBuf)!= HAL_OK)

        {

            //Error_Handler();

        }

            

        while (UartReady != SET)

        {

          

        }

          aRxBuffer[0]='a';

          

       }

          

  }

Help me guys with some solution.

my MCU need to reply back CIAO whenever I receive PIP on the UART.

Please have a look at the image.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0