cancel
Showing results for 
Search instead for 
Did you mean: 

GP and N version ICs

PPate.1
Associate III

Hi,

I am using STM32C071CBT6 chip on my custom board. From datasheet, i could see that there are two versions available - GP and N version. Part number section of datasheet mention about 3 more characters after this part no. to identify if it is N version. 

PPate1_0-1743594616574.png

Does above description means that there will be letter 'N' at the end of part no. to identify it as N version? And if no letters are present after part no. (i.e. blank ) means it is GP version? 

My chip on board is as below:

PPate1_1-1743594767820.jpeg

Am i right that this is GP version chip and not N version?

Thanks,

Pradeep

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Correct, the version ‘N’ would have the marking 71CBT6N at the 2nd line, while ‘GP’ only contains 71CBT6. The marking is therefore structured similarly to the order designation that you had inserted.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Correct, the version ‘N’ would have the marking 71CBT6N at the 2nd line, while ‘GP’ only contains 71CBT6. The marking is therefore structured similarly to the order designation that you had inserted.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.