cancel
Showing results for 
Search instead for 
Did you mean: 

Getting Started...

rmeghdies9
Associate
Posted on December 29, 2011 at 06:34

Product: STM3240G-EVAL

Microcontroller: STM32F407IGH6

IDE: Atollic's TrueSTUDIO Lite IDE

I wrote a simple program however, every time I click ''run'' I get a msg box saying, ''the selection cannot be launched, and there are no recent launches''.

Any ideas?

Your help would be much appreciated.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
rmeghdies9
Associate
Posted on April 03, 2012 at 06:08

For anyone else with the same problem.

I solved the issue by changing the debugger to ''ST-Link Debugger''.

For some reason it defaulted to another one.

fullcaos
Associate II
Posted on October 06, 2012 at 11:44

Hi, I just bought an evaluation board STM3240G-EVAL

I tried to modify the example provided by ST called ''ADC3_DMA'' but I could not change the pin from what I acquire the signal

For example I wanted to go from pin PF9 to PC4 and I modified the GIPIOF in GPIOC and pin number GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 as GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

but it does not work ....

I attached the main file in this post.

________________

Attachments :

main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1D3&d=%2Fa%2F0X0000000bju%2FiJuqj.iR320oSY8HMafLHfocRVaRxLjV32CHlLfU4k8&asPdf=false