2009-09-08 2:21 AM
GDB issue on STM32
2011-05-17 4:23 AM
Hello everybody,
I am working on a STM3210E-EVAL board for 2 weeks now and there are some odd things happening when I use the GDB provided with WinARM(gdb version 6.4.50.20060226-cvs). I use Eclipse as a IDE, everything seems to be working fine until I reach some instructions that need to work with register R7('mov.w r7,0' or 'mov.w r7,r7,#12', also an add.w r7 creates the same outcome), I took a look on the packages sent by gdb and this is what it sends: Sending packet: $m2000037e,2#8c...Ack Packet received: 80bc Sending packet: $m20000380,2#58...Ack Packet received: 7047 Sending packet: $Hc0#db...Ack Packet received: Sending packet: $s#73...Ack Packet received: O7461726765742073746174653a2068616c7465640a Packet received: O7461726765742068616c74656420696e205468756d622073746174652064756520 746f2073696e676c6520737465702c2063757272656e74206d6f64653a205468726561 64200a785053523a20307830313030303030302070633a20307832303030303332320a target state: halted target halted in Thumb state due to single step, current mode: Thread xPSR: 0x01000000 pc: 0x20000322 Packet received: T05 Sending packet: $g#67...Ack Packet received: 0000000000000080e04f0020020000003600000037000000ffffbff700000000 ffffffffffffbff73d0000006dddfe4810000000bc4f00204d26002023030020000000000 0000000000000000000000000000000000000000000000000000000000000000000000000 0000000000000000000000000000000000000000000000000000000000000000000000000 00000000000000000000000000000000000000000000000000001 Sending packet: $m20000322,4#56...Ack Packet received: 07f10c07 Sending packet: $m3c,4#63...AckPacket received: E0E The bolded message is what actually this error is about, normally that package should not exist and it happens only when I try ''mov.w r7,0'', if I try ''mov.w r1,0'' this packet doesn't get sended. Everything works fine(single stepping,watches,and so on) except for this problem. Any ideas? Thank you in advance! LC [ This message was edited by: al2757 on 08-09-2009 14:52 ]