cancel
Showing results for 
Search instead for 
Did you mean: 

[FYI] Devboard demo binaries are no longer packed with Cube

waclawek.jan
Super User

In latest CubeL4 v1.14 release notes I noticed this:

 * Demonstrations binaries are no more delivered within the STM32CubeL4 MCU package. They are available for download, in addition to their required media files if any, in a standalone package accessible through each hardware board official webpage. Please refer to the corresponding demonstration binary readme.txt to get webpage for each board.

Indeed, looked at the 'L476 Disco's site, and it's under Resources/Compiled demos. I guess/hope this will be the same with other devboards.

ST: It would be nice if the corresponding sources would be packed with the demo, and in case there are historical versions of the demo (e.g. both SPL and Cube based), then if you'd post all of them.

JW

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0