cancel
Showing results for 
Search instead for 
Did you mean: 

fsmc and nand flash

jbl_raw
Associate II
Posted on January 11, 2013 at 02:12

1-i'm confused in datasheet i see 4x64mb per bank . it's means maximum of  each nand flash is 64mbyte .

2- in the AN2790 Application note  about lcd with fsmc.

read from NAND Flash 11 fps

read fron sd card   12fps

why the sd card faster than nand flash sd card is serial and. nand flash  is parallel

and read time is 25ns per byte it means 40mbyte per second read speed.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on January 21, 2013 at 01:00

You'd need to describe the regions of memory in your GUI, scatter file or linker script. You'd define sections within these regions, and then direct the compiler to place specific functions or objects within those sections.

To program the code into these memories you'd need to tell your debug tools about how to write into the NOR via an applet or macro. You could also do it yourself (provide routines to download), or use something like J-Flash

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..