2022-07-20 11:14 PM
I'm using Nucleo-G474RE + X-Nucleo-GFX01M2
I downloaded the X-Cube-DISPLAY package
I cannot find a flash loader file for the Nucleo-G474RE in the ExternalLoader folder. See below screenshot
Where to find an ExternalLoader file or can I use one of the below ones?
2022-08-01 4:43 AM
2022-08-01 5:09 AM
in-line images not visible via posting method, post to forum directly, not via email reply.
I did test on NUCLEO-G474 and GFX board.
File needs to be in bin/ExternalLoader directory
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.