cancel
Showing results for 
Search instead for 
Did you mean: 

F030中关于SPI multi master,我一直无法实现多主机通信的问题。

燕赵.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

> Regarding the SPI multi master in F030, I have been unable to realize the problem of multi-master communication

This is not enough information to help.

SPI is typically a single master system in order to prevent two chips from driving the same line.

If you feel a post has answered your question, please click "Accept as Solution".