cancel
Showing results for 
Search instead for 
Did you mean: 

example with HAL_FLASHEx_Erase_IT

Henry Brasil
Associate II
Posted on January 12, 2018 at 09:28

hi, I know the way to use HAL_FLASHEx_Erase() in my main loop and it works,erasing some flash areas.

Now I want to use the HAL_FLASHEx_Erase_IT() , I have enabled from the cube the flash global interrupt,

Do I have to put it inside of the flash global interrupt? or not, 

can you tell me the way to use the it ?or write me down a simple example

thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0