cancel
Showing results for 
Search instead for 
Did you mean: 

Do we need to enable and set SVCall, PendSV priorities ?

ranran
Senior II

Hello,

In stm32cubemx generated code there is the following routine.

void HAL_MspInit(void)
{
  /* USER CODE BEGIN MspInit 0 */
 
  /* USER CODE END MspInit 0 */
 
  __HAL_RCC_SYSCFG_CLK_ENABLE();
 
  HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
 
  /* System interrupt init*/
  /* MemoryManagement_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(MemoryManagement_IRQn, 0, 0);
  /* BusFault_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(BusFault_IRQn, 0, 0);
  /* UsageFault_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(UsageFault_IRQn, 0, 0);
  /* SVCall_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SVCall_IRQn, 0, 0);
  /* DebugMonitor_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DebugMonitor_IRQn, 0, 0);
  /* PendSV_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(PendSV_IRQn, 15, 0);
  /* SysTick_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);
 
  /* USER CODE BEGIN MspInit 1 */
 
  /* USER CODE END MspInit 1 */
}

Yet, in examples used (also with freeRTOS), I don't find similar initializations of priorities for this IRQs.

Is it really needed ? Why is it missing in examples ?

Thank you,

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.