cancel
Showing results for 
Search instead for 
Did you mean: 

dfu-util 0.6 available (win32, Ubuntu and Mac ppc binaries)

stforum.tormod9
Associate II
Posted on May 26, 2012 at 11:28

With the latest release of dfu-util (which supports DfuSe devices since 0.5) we also offer Win32 and Mac (ppc) binaries at

http://dfu-util.gnumonks.org/

For a DfuSe usage example (and a link to Ubuntu binaries) please see

http://www.seeedstudio.com/wiki/index.php?title=Dfu-util

dfu-util can be used for downloading (and uploading) firmware instead of ST's ''DfuSe Demo'' application. Note that you will have to uninstall the ST driver and register the libusb driver with WinUSB. This is explained in the README.txt inside the win32 zip file. The binaries were tested on Windows 7 64bit.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0