cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Corrupts OpenSTM32-Eclipse-Project when rebuilding

manuel239955
Associate II
Posted on September 23, 2015 at 10:15

Hello,

i have a serious problem with project regeneration with CubeMX.

After regenerating a project, the linked files (for example HAL and configuration files, like main.c) point to the wrong direction. The file links still has the right name (''adc.c'' but points to/opens a wrong file (for example, all file links generated by CubeMX point to the first file found, like adc.c or startup_stm32f746xx.s. This is very annoying. Is this a known bug? Any workaround besides deleting the project and adding custom libs/includes every time?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1