cancel
Showing results for 
Search instead for 
Did you mean: 

Cubemx code generation bug for LL USART RX Active level Inversion

David Fisher
Associate II
Posted on October 17, 2017 at 19:04

The code generated for an F303CCTx LL Active level Inversion of USART1 RX is :-

LL_USART_SetRXPinLevel(USART1, UART_ADVFEATURE_RXINV_ENABLE);

which doesn't compile. Where as I think it should be :-

LL_USART_SetRXPinLevel(USART1, LL_USART_RXPIN_LEVEL_INVERTED);

The TX doesn't have this problem.

I also found that I need to add :-

 /* Enable RXNE and Error interrupts */

LL_USART_EnableIT_RXNE(USART1);

LL_USART_EnableIT_ERROR(USART1);

to enable the interrupts I need. As it would seem the best place to add these is in the MX_USART1_UART_Init function that is generated, would it be possible to add a user code section at the end of the function to add this code to. 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Jeanne Joly
Senior III
Posted on February 08, 2018 at 14:50

Hello

Fisher.David.003

,

Sorry for my late reply.

This issue is now solved. Please, update your CubeMX release with the current one (CubeMX-4.24).

BR. Jeanne

View solution in original post

2 REPLIES 2
Imen.D
ST Employee
Posted on October 20, 2017 at 14:16

Hi,

Your reported issue is raised internally for further investigation.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on February 08, 2018 at 14:50

Hello

Fisher.David.003

,

Sorry for my late reply.

This issue is now solved. Please, update your CubeMX release with the current one (CubeMX-4.24).

BR. Jeanne