cancel
Showing results for 
Search instead for 
Did you mean: 

CRC module

tibo
Associate II
Posted on September 19, 2008 at 10:53

CRC module

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tibo
Associate II
Posted on May 17, 2011 at 12:45

I want to use the CRC module with DMA: copying a memory block with DMA to the

CRC engine and getting back the CRC result. With the ''memory-to-memory''-mode

of the DMA controller this should be possible.

RM0008, page 43 says: ''The CPU is stalled during the computation (of the CRC),

thus allowing back-to-back write … without software wait cycles.''

My question:

Is it possible to use the DMA controller with CRC and is the DMA controller stalled

during the computation (otherwise the result will be perhaps not correct)?

Is it possible to use the cpu during the computation or is it also stalled?