2016-09-26 1:41 AM
Dear All,
I need to make BCD 4 digit in 7-segment display.
My spi recieved data is 14 bit, take a look this sample code in another MCU.
void toBCD(int16 val,int8 * buff) {
//converts 16bit value, to five BCD digits. Tries to do it fairly
//efficiently, both in size, and speed.
int1 temp_bit;
int8 nibctr;
buff[0]=buff[1]=buff[2]=0;
do {
if ((buff[0] & 0xF)>=5) buff[0]+=3;
if ((buff[0] & 0xF0)>=0x50) buff[0]+=0X30;
if ((buff[1] & 0xF)>=5) buff[1]+=3;
if ((buff[1] & 0xF0)>=0x50) buff[1]+=0X30;
if ((buff[2] & 0xF)>=5) buff[2]+=3;
temp_bit=shift_left(&val,2,0);
shift_left(buff,3,temp_bit);
} while (val!=0);
}
void main() {
int16 val;
//three bytes for packed BCD result
int8 buff[3];
setup_adc_ports(NO_ANALOGS);
setup_adc(ADC_OFF);
setup_psp(PSP_DISABLED);
setup_spi(FALSE);
setup_timer_0(RTCC_INTERNAL|RTCC_DIV_1);
setup_timer_1(T1_DISABLED);
setup_timer_2(T2_DISABLED,0,1);
val=12345;
toBCD(val,buff);
//At this point, the three bytes will contain:
// 45
// 23
// 01
while (true);
}
1. How can I implement this idea in RTC application?
2. Is it possible to apply this link ..http://embedded-lab.com/blog/stm32s-internal-rtc/
Kindly help me.
Refference code is required.
2016-09-26 5:54 AM
Couldn't one just use %10 and /10 to convert an integer into decimal digits? Also itoa() and sprintf()? For BCD digits %16 and /16 to free the individual 4-bit nibbles containing them.
The STM32 should provide a BCD and binary RTC mode.2016-09-26 6:04 PM
long Dig_0, Dig_1, Dig_2, Dig_3, Dig_4;
void bin_to_Dig(long bin_inp)
{ // This is for VK3UM program
long temp; // 16 bit binary to BCD 5 byte
int nibh;
int nibl;
temp = bin_inp / 18.2041667; // make into binary degrees value
//Dig_4 = temp/10000; // This is not needed as just 4 digits
//temp = temp - (Dig_4 * 10000); // this will always be zero
Dig_3 = temp/1000;
temp = temp - (Dig_3 * 1000);
Dig_2 = temp/100;
temp = temp - (Dig_2 * 100);
Dig_1 = temp/10;
temp = temp - (Dig_1 * 10);
Dig_0 = temp;
nibh = Dig_1; // MSB BYTE This is the 2nd digit
nibl = Dig_2; // LSB BYTE This is the 1st digit
CountMSB = (nibl|(nibh<<4));
nibh = Dig_3; // MSB BYTE This is the 3rd digit
nibl = Dig_0; // LSB BYTEs This is the 0rd digit, .1 value
CountLSB = (nibl|(nibh<<4));
or this is also meaningful in case of data buffer selection,void bin_to_Dig(int16 bin_inp,int8 * buff){
//converts 16bit value, to five BCD digits. Tries to do it fairly
//efficiently, both in size, and speed.
int8 nibh;
int8 nibl;
int1 temp_bit;
int8 nibctr;
buff[0]=buff[1]=buff[2]=0;
do {
if ((buff[0] & 0xF)>=5) buff[0]+=3;
if ((buff[0] & 0xF0)>=0x50) buff[0]+=0X30;
if ((buff[1] & 0xF)>=5) buff[1]+=3;
if ((buff[1] & 0xF0)>=0x50) buff[1]+=0X30;
if ((buff[2] & 0xF)>=5) buff[2]+=3;
temp_bit=shift_left(&bin_inp,2,0);
shift_left(buff,3,temp_bit);
} while (bin_inp!=0);
nibh = 0; //buff[0] >> 4; // buff 0 (1) msnibble = 2nd digit
nibl = 0; //buff[1] & 0x04; // buff 1 (2) lsnibble = 1st digit
CountMSB = (nibl|(nibh<<4; // buff 1 (1) msnibble = 3nd digit
nibl = 0; //buff[0] & 0x04; // buff 0 (0) lsnibble = 0 digit
CountLSB = (nibl|(nibh<<4));
2016-09-28 2:18 PM
2016-10-23 7:02 PM
Dear Sir Clive,
I need your kind attention here. In response to your comment ''The STM32 should provide a BCD and binary RTC mode.'' 1. Are you talking aboutAN3371Application note? 2. STM32 has a BCD counter/timer, people using in this way,http://embedded-lab.com/blog/stm32s-internal-rtc/ 3. Dont you think I need to proceed unit32_t spi data to make BCD in this way?uint32_t dec2bcd(uint16_t dec) { uint32_t result = 0; int shift = 0; while (dec) { result += (dec % 10) << shift; dec = dec / 10; shift += 4; } return result;}/* Recursive one liner because that's fun*/uint32_t dec2bcd_r(uint16_t dec){ return (dec) ? ((dec2bcd_r( dec / 10 ) << 4) + (dec % 10)) : 0;}Kindly help me.
2016-10-24 12:08 PM
The RTC library code can handle binary or BCD usage.
Not sure the value if citing whole web pages, what specifically in the page is an issue here? Posting code without supporting subroutines isn't helpful. Let's restate what the real issue is here. Your have 1234 decimal and you want a some BCD representation as either a) 0x1234 b) Two bytes 0x12 and 0x34 c) Four bytes 0x01, 0x02, 0x03, and 0x04 d) Four bytes 0x30, 0x32, 0x33 and 0x34, ie ASCII string ''1234'' Assuming Cint x = 1234; // some 14-bit value
unsigned char c[4]; // 4 digits
c[0] = (x / 1000) % 10;
c[1] = (x / 100) % 10;
c[2] = (x / 10) % 10;
c[3] = x % 10;
I understand the 7-segment implementation, I really don't understand where the RTC request is coming from, or what SPI device is sending what. You're mixing up a bunch of different thoughts here, you need to provide more clarity, stated in your own words/diagrams.
2016-10-24 12:15 PM
This user trying to make UART data to 4 digit display. In case of SPI data, if uint8_t pDataRx[4] is turned to BCD and fed them in 74HC4511 decoder-driver to 4 digit display. It will work? Further translation is needed or not?
Present the data you are receiving, and what you want/expect to be displayed, provide multiple examples.
https://www.sparkfun.com/datasheets/IC/74HC4511.pdf
2016-10-24 12:20 PM
int y = 0x1234; // some 4 digits in BCD
unsigned char e[4]; // 4 digits
e[0] = (y >> 12) % 16;
e[1] = (y >> 8) % 16;
e[2] = (y >> 4) % 16;
e[3] = (y >> 0) % 16;
2016-10-24 7:39 PM
2016-10-26 2:30 AM
Forgive me, but I am curious. Why on earth do you need to use BCD in the 21st century?