cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting to TMS320 Host Port Interface via FSMC

colinh
Associate II
Posted on September 01, 2010 at 15:51

Connecting to TMS320 Host Port Interface via FSMC

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
raptor483
Associate
Posted on May 17, 2011 at 14:05

I would also love to know the asnwer. Did you found out anything?

I need to interface 8 bit SRAM with FSMC. It's address bus is connected through latches, so I need multiplexed access (like NOR memory type). But in ref-man, this combination is not stated in table NOR Flash/PSRAM supported memories and transactions.  Everything have 16 bit memory data size :-(. Is there any possibility to use this type of SRAM connection?

MCU: STM32F103VET6

SRAM: R1LV0408CSA

Signals on SRAM:

A[00-15] multiplexed

A[16-18] direct

D[0-7] direct

CS, OE, WE direct

Thanks, Viktor