Question
Compatibility for stm32l031f6 with STMFlashLoader.exe
Hi,
I am currently using the stm32l031f6 which is a 32K memory device and I am trying to use the STMFlashLoader.exe, which is the command line version of the flash loader, to download firmware into the device. However, in the map directory for the STMFlashLoader.exe, for L0 devices, there is only "STM32L0_x3_x2_x1_64K.STmap" and "STM32L0_x3_x2_x1_192K.STmap". Yet, the stm32l031f6 is a 32K memory device. Do you have any STmap file for my device?
Thank you,
Matt