cancel
Showing results for 
Search instead for 
Did you mean: 

Comments on Breakout board for STM32

vindhyachal
Associate II
Posted on April 23, 2016 at 14:26

I have made a schematic of breakout board for STM32F205RBT6.

I will make a square board with all pins from MCU coming out to outer 2.5mm headers.

1. Symbols in schemtaic with name ''Nx'', are bascially are small jumpers with 0805 size.

2. I have some odd debug connector here. I have made this kind of connection for other boards so that's not a problem.

Any comments/suggestions on ckt.

Here is ckt:  http://docdro.id/kECPFgT
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Radosław
Senior III
Posted on April 23, 2016 at 20:51

Hello.

1. check waveshare boards.

2. put VCC and especially OSC pin to headers will maybe bring EM noices.

re.wolff9
Senior
Posted on April 24, 2016 at 08:30

.... so consider putting a jumper (Nx) that allows you to interrupt the oscillator pins going to the header. 

You can also cheat by looking at schematics for ''discovery'' boards, and the nucleo.  The nucleo is complicated because a single PCB supports many different CPUs.