2015-09-30 6:21 AM
CAN SOMEONE PROVIDE ME WITH FULL WORKING CODE OF RX AND TX BUFFER FOR RECEIVING AND TRANSMITTING DATA IN STM32F07 USART.
ANY HELP IS WELCOME.THANKS IN ADVANCE2015-09-30 12:10 PM
Show us what you have completed so far and where you are getting errors.
If you are only looking for a programmer to write code for you then your best option is to run a help want ad on a local website or newspaper, stating the skills you need to hire and what pay rate you will offer. Have you looked at the ST code examples? Jack Peacock2015-10-01 1:15 AM
Hi kazi.adeem,
I agree with Jack's point of view.Any way, I suggest you take examples available inhttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260612
as a start point to develop your own application.You may find examples in this folder after downloading the package: STM32Cube_FW_F0_V1.4.0\Projects\STM32F070RB-Nucleo\Examples\UART.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.