2018-04-30 6:41 PM
Has anyone seen this warning while using FreeRTOS? The full define is :
#define osThreadDef(name, thread, priority, instances, stacksz) \
const osThreadDef_t os_thread_def_##name = \{ #name, (thread), (priority), (instances), (stacksz)}This define is being used because the current FreeRTOSConfig.h has configSUPPORT_STATIC_ALLOCATION == 0. This was taken from the tcpip RTOS example from H7_V1.2.0.
Has anyone seen this?
2018-09-07 1:52 AM
I have seen this problem when using static timers, specifically with the osTimerStaticDef macro, but my experiences may be of help to you or others.
static osTimerId IdleTimerId ; // This is the timer handle
osStaticTimerDef_t IdleTimerControlBlock; // This is some ram for the timer
osTimerStaticDef(IdleTimer, IdleTimer_TimeOut, &IdleTimerControlBlock); // This macro creates a timer object
Here is the macro itself:-
#define osTimerStaticDef(name, function, control) \
const osTimerDef_t os_timer_def_##name = \
{ (function), (control) }
#endif
And this is what it creates the following :-
const osTimerDef_t os_timer_def_IdleTimer = { IdleTimer_TimeOut, &IdleTimerControlBlock };
IdleTimer_TimeOut is a callback function pointer, &IdleTimerControlBlock is a pointer to the TCB
I had the callback function declared as follows:-
void IdleTimer_TimeOut(void)
and got the warnings you mentioned. So I inspected the definition of osTimerDef_t
typedef struct os_timer_def {
os_ptimer ptimer; ///< start address of a timer function
osStaticTimerDef_t *controlblock; ///< control block to hold timer's data for static allocation; NULL for dynamic allocation
} osTimerDef_t;
and then os_ptimer
typedef void (*os_ptimer) (void const *argument);
You can see that the call back pointer needs to correspond with this type. I changed the call back declaration as follows and the warnings went away.
void IdleTimer_TimeOut(void const *argument)
Hope this helps.