2010-08-03 7:22 AM
Checksum (EWARMv5)
2011-05-17 5:00 AM
Thanks for that URL. I liked this part
''In EWARM 5.50
This ability is not documented and it can only be invoked as a command line option.'' I started with EWARM 5.30, over a year ago, and now have EWARM 5.50.5 as well. Nice to know that IAR (somewhat) supports the STM32 CRC generator.2011-05-17 5:00 AM
With version 6.10 it works with the tool settings for checksum calculation.
Check Fill unused memory, use 0xFF
Generate checksum 4 bytes, Alignment 4, CRC32 Complement: As is Bit order: MSB first Check the ''Reverse byte order within word'' flag. Initial value: 0xFFFFFFFF, uncheck ''Use as input'' And of course, do not forget to set the start and end addresses. Have fun, Dreeke