Cannot read config register value of M24LR16E via I2C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-06-07 12:34 AM
Hi All,
I'm trying to communicate with M24LR16E(NFC tag IC) via I2C (STM32F103R is Master)
I could find configuration register(address 2320) has initial value 0xF4.
so I tried to read the configuration register, but I got 0xFF.
would you please take a look at what is wrong with my code ?
=======================
uint16_t NFC_sys_addr = 0xAE, nfc_conf_addr=2320;
uint8_t nfc_config=0;HAL_I2C_Master_Transmit(&hi2c1, 0xAE, (uint8_t *)&nfc_conf_addr, 2, 100); // set config register address
HAL_I2C_Master_Receive(&hi2c1, 0xAE, (uint8_t *)&nfc_config, 1, 100); // read byte printf('NFC config 0x%x\r\n', (unsigned int)nfc_config);========================
Thanks in advance
Best Regards,
Hae Ryong
#i2c-isues #m24lr16e- Labels:
-
I2C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-06-07 2:32 AM
I verified following code working fine
=================
uint16_t NFC_sys_addr = 0xAE, nfc_conf_addr=2320;
HAL_StatusTypeDef i2c_status=HAL_OK; uint8_t i2c_wBuf[3]; uint8_t i2c_value=0;i2c_wBuf[0] = (uint8_t)((nfc_conf_addr&0xFF00) >> 8);
i2c_wBuf[1] = (uint8_t)(nfc_conf_addr&0x00FF);i2c_status = HAL_I2C_Master_Transmit(&hi2c1, NFC_sys_addr, (uint8_t *)i2c_wBuf, 2, 100);
HAL_Delay(10); i2c_status = HAL_I2C_Master_Receive(&hi2c1, NFC_sys_addr, (uint8_t *)&i2c_value, 1, 100); printf('NFC value 0x%x at 0x%x, status=%d\r\n', (unsigned int)i2c_value, nfc_addr, i2c_status);==================
I could see i2c_value is 0xF4
I guess
nfc_conf_addr value should be converted to i2c_wBuf[] for HAL_I2C_Master_Transmit() and HAL_I2C_Master_Receive()
Thanks anyway.