cancel
Showing results for 
Search instead for 
Did you mean: 

CAN

steve3
Associate II
Posted on September 19, 2008 at 04:35

CAN

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
steve3
Associate II
Posted on May 17, 2011 at 12:38

Hello all,

Has anyone got the ST sample code for the STM32F10X-12K-EVAL board working. By which I mean remapping the alt function to PD0, PD1, correcting the baud rate calculations, and with CAN_Mode=CAN_Mode_Normal, and actually receiving data on the bus?

If you have then I would greatly appreciate seeing the working code.

Regards

Steve

smart
Associate II
Posted on May 17, 2011 at 12:38

see this...

http://www.st.com/mcu/forums-cat-6876-23.html

steve3
Associate II
Posted on May 17, 2011 at 12:38

Thanks for your reply. Yes I've read that with interest, I'm doing all these things, Baud rate correction, remap pins, can clock, port D clock.

I notice that when the TX pin is set up as AF_PP it outputs a 0, which seems to silence the can bus, CAN H goes and remains high, which does not look right to me. I'm only trying to receive data, so I cna configure the pin as input pullup, then the CAN signals continue, but I get no RX.

I'm puzzeled.

Steve

steve3
Associate II
Posted on May 17, 2011 at 12:38

I look again...

One problem solved, I was not enabling alt function clock, now that I do, I do not kill the bus signal when I have TX as AF_PP.

But I still do not receive

Steve

steve3
Associate II
Posted on May 17, 2011 at 12:38

Yahoo, I can now TX and RX.

Problems were all in the ST sample code.

1)Baud rate calculations

2)Flash latency not set up correctly

3)AF clocks not enabled

Soon le weekend

jussi
Associate
Posted on May 17, 2011 at 12:38

Hello,

Suprisingly I'm having same problem...

Is this flash latency set up relevant and if so how it's done?

I just keep wondering how ST releases this kind of example code.. :-[

-Jussi

chesneje
Associate II
Posted on May 17, 2011 at 12:38

Hi,

I have the same problem. Can you send me your configuration code.

Thanks.

muhammaduzairafzal45
Associate III
Posted on December 19, 2012 at 14:53

working code of mine:

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32%20CAN%20Filter&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=4]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32%20CAN%20Filter&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=4

Just change  CAN_InitStructure.CAN_Mode value to CAN_Mode_Normal to communicate

externally. Correct Baud rate setting is very important for CAN..small mistake in calculating it

might result in communication error.