cancel
Showing results for 
Search instead for 
Did you mean: 

Can't connect to Discovery card

LMI2
Lead
Posted on June 27, 2015 at 17:52

Just after I downloaded a program into Stm32F100 Discovery card, the STM32 ST-LINK Utility lost contact with the card. Now it cannot connect to it, no matter what I do. The software in the card is a plain GPIO test from Cube, but it may initialize all IO pins.

If the HW is working, is there an way to reprogram the chip. Or an other way to see what is wrong.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
LMI2
Lead
Posted on June 28, 2015 at 00:54

I got it working. I had to keep the reset button pressed when I started the STlink utility.

Posted on June 28, 2015 at 01:19

See also ''Connect under Reset'' and BOOT0 Pulled High

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
LMI2
Lead
Posted on June 28, 2015 at 01:36

Thank you for the advise.

I could not find the ''Connect under Reset'' option. Is it unavailable because the built in ST link is version 1? There are only Normal and Hot Plug modes available.