cancel
Showing results for 
Search instead for 
Did you mean: 

can speed problem at cpu 8 Mhz

ozenozkaya
Associate II
Posted on June 26, 2009 at 08:02

can speed problem at cpu 8 Mhz

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ozenozkaya
Associate II
Posted on May 17, 2011 at 13:16

I want to process the CPU at 8 Mhz. I encountered no problems till that value (it works fine at 64 and 16 mhz values) when i try 8 Mhz, CAN bus couldnt carry info. by the way, does it help if i set the prescaler as 0. what does it mean? i found no info about 0 prescaler in the manual. how i can get rid of this problem? thanks and regards..

/* HCLK = SYSCLK */

RCC_HCLKConfig(RCC_SYSCLK_Div1);

/* PCLK2 = HCLK/2 */

RCC_PCLK2Config(RCC_HCLK_Div1);

/* PCLK1 = HCLK/2 */

RCC_PCLK1Config(RCC_HCLK_Div1);

/* PLLCLK = 4MHz * 4 = 16 MHz */

RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_4);

// can regulations:

CAN_InitStructure.CAN_SJW=CAN_SJW_1tq; //1

CAN_InitStructure.CAN_BS1=CAN_BS1_8tq; //8

CAN_InitStructure.CAN_BS2=CAN_BS2_7tq; //7

CAN_InitStructure.CAN_Prescaler=1;