cancel
Showing results for 
Search instead for 
Did you mean: 

Can FSMC request stops processor?

jaroslaw2
Associate II
Posted on August 07, 2008 at 08:13

Can FSMC request stops processor?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jaroslaw2
Associate II
Posted on May 17, 2011 at 12:41

Hi,

I would like to use FSMC in Motorola 6800 (M68) mode to drive graphical LCD (KS0108).

My square signal form PWM output is more important than LCD. I wonder if FSMC request for data from the LCD will pause a core processor for another operation? The memory transaction last max. 3.8 us so the square signal can be distorted.

Second question is proposition of connection FSMC as M68. Why you didn't propose to use NADV signal to use it as strobe. Your proposition will cause a hazard? Did somebody test M68 mode to drive for e.g. LCD.

thnaks,

J.O.