cancel
Showing results for 
Search instead for 
Did you mean: 

Build STM322xG EVAL FW with yagarto

dimax
Senior
Posted on November 12, 2012 at 11:23

HI,

Is where any makefile or ready project to build STM322xG_EVAL FW with yagarto or GNUARM?

I have downloaded

STM32F2-F4_Demonstration_Builder_V1.0.1

but it has no plain Makefile for GCC. I wonder if someone can share it with us.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Posted on November 29, 2012 at 21:18

Jan's point is that your failure description is ambiguous, the code does in fact compile and link, the problem is what happens when it runs. The description needs more specificity to what failed, and how, which you might be able to answer if you ran the code on a debugger, and did some basic bisection.

If it hard faults, what code is faulting..... If it gets stuck in some loop, which one..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dimax
Senior
Posted on November 30, 2012 at 11:27

Sorry did not think this way.

Well All I can see is that there is nothing on LCD. It stays same as it was at reset and boot time. I do not have a debugger so I can't look inside right now. I plan to install openOCD and run debugger via ST-Link but not sure when will I have time to do it.