cancel
Showing results for 
Search instead for 
Did you mean: 

bug in STM32 LWIP in IAP example?

dieter 123
Associate III
Posted on September 07, 2017 at 08:07

could it be that in STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAP

the latest firefox is not supported?

FW download via internet explorer works but but not firefox 55.0.3 (32-Bit) !

Thx

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
dieter 123
Associate III
Posted on November 22, 2017 at 10:10

HAJJEM.Oussema

Can you comment on this issue?

The ST is code in this project is meant to work with firefow as well. But it doesnt!

Same applies to google chrome browser

Is ST going to fix this?

Posted on November 23, 2017 at 10:58

Hello,

I confirm that some regressions are available when using last Firefox versions, this will be reported to be fixed in the next STM32CubeFW F4 releases.

Thanks and regards,

Oussema.