cancel
Showing results for 
Search instead for 
Did you mean: 

Bluetooth firmware update

Max Veen
Associate II
Posted on July 18, 2017 at 11:00

Hi all,

For a project we have to update the firmware of the STM32F469xx over the air by a Bluetooth connection

with a transmitter (can that be a smart phone?) and receiver on the microcontroller device part.

In an article I have read about such a possibility where an Android phone was used to perform the update

to the microcontroller.

I like to know several things:

1. Can I adapt the bootloader code of this microcontroller to support application firmware update via bluetooth.

    Which steps do I have to perform to achieve this? Are there any guidelines for this?

2. In what way can I secure this firmware update over the air via bluetooth?

Any help I will appreciate!

Thanks in advance

Max

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0