cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG - simultaneously Master&Slave

ann
Associate II

i want to use a board as master and slave simultaneously.  role= GAP_PERIPHERAL_ROLE | GAP_CENTRAL_ROLE; 

now, i am able to establish a connection between a Master&Slave board and a slave board. however, when i want to set the Master&Slave board into discoverable mode after that,

 an error occurs: error code is 0x0C BLE_ERROR_COMMAND_DISALLOWED .

Why is that? and how to solve this problem?

if i set the device into discoverable mode directly (do not connect it with slave A), the command was successfully.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
embedded_guy
Associate

Hi,

Not sure if you resolved this, but I'm seeing something similar...I think.

I am setting up my advertising packet with extended (custom) information. I have seen that if I use more than one advertising data handle when calling aci_gap_set_advertising_enable, I get that error as well (0x0C DISALLOWED). If I only send in one handle, then the enable command doesn't return an error.

However, I have also seen that the slave module will still connect, even with this error returned.

Let me know if you were able to figure this out.

Thanks,

Anthony