2016-06-16 6:16 AM
I am working with the Discovery Development Board (STM32F407) and I would like to have functions for the 16-bit timers that looks like this:
void
startTimer(uint32_t timeoutMs, EventCallback_t timerInterruptCallback)
I'm currently using the formula below, but I recently discovered and corrected an overflow problem that makes this algorithm pretty bad (the error is less than 1% for timeout values below 800 ms at 32 MHz timer clock, but above that it gets pretty bad). I don't want to use floating point mathematical operations or lookup tables. Does anyone have any clever ideas?
clockFreqBeforeDivision = GET_TIMER_FREQ(TIM2);
perfectClockFreqAfterDivision = (((uint32_t)(1000 * 65536)) / ((uint32_t)milliseconds));
divisor = 1 + (clockFreqBeforeDivision / perfectClockFreqAfterDivision);
actualClockFreqAfterDivision = clockFreqBeforeDivision / divisor;
timerPeriod = milliseconds * (actualClockFreqAfterDivision / 1000);
2016-06-16 7:34 AM
Does anyone have any clever ideas?
Here's a paradigm shifting thought, TIM2 is 32-bit, drive it as a high frequency, free running time base, with a maximal count and set the timeout interrupt by programming the TIM2->CCRx X milliseconds ahead of current TIM2->CNT At 72 MHz the wrap time is about a minute, right? At 1 MHz you'd have over an hour range. For period/prescaler stuff you are factoring into two integers, generally you'd want the prescaler to be the smaller of the two, as you want the period to be more that 1 or 22016-06-16 10:28 AM
I estimate that I will need at least 8 timers so I must use some 16-bit timers.
2016-06-16 12:34 PM
Each timer has 4 channels, you could also manage a list of upcoming events and sequence them.
People often manage a long list of events and hand-off during the 1KHz (1ms) ticker as each expires.2016-07-12 4:07 AM