ARD-OTTO-STM32: First Arduino board based on STM32 ARM® Cortex®-M MCU
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-05-20 9:03 AM
Posted on May 20, 2016 at 18:03
STAR Otto presents to the Arduino environment exceptional performance from the 32-bit STM32F469 MCU thanks to:
STMicroelectronics and Arduino Launch Cooperation to Expand Maker-Community Access to STM32 MCUs and Sensors
is the first product of the STAR (ST and Arduino) program. It is the first Arduino�board including high-performance graphics, display support, and Wi-Fi link to enable users to create connected systems with amazing visual and audio experience.
- ST�s Chrom-ART� graphics accelerator
- MIPI DSI display interface
- Open-source software graphics library
- Pre-integrated wireless link and audio capabilities, enabled by an ST MEMS microphone together with the necessary open-source drivers
http://www.st.com/content/st_com/en/about/media-center/press-item.html/t3829.html
#ard-otto-stm32To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0