cancel
Showing results for 
Search instead for 
Did you mean: 

__ADCX_FORCE_RESET() not seen

keaven
Associate II
Posted on August 03, 2015 at 16:58

I am using the version 1.3.1. of stm32f4xx hal drivers. I am using the 3 ADCs. ADC1 and ADC2 in dual mode DMA interrupt driven and ADC3 regular conversion.

As you can in the code below I am using the functions __ADCx_FORCE_RESET() (x= 1, 2, and 3) . I dont understand why but the functions don't link. I get undefined symbol. I must use __ADC_FORCE_RESET() to get it work but it will reset all ADCs which I don't want. Any ideas why? Thank you

void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc)
{
if(hadc->Instance == ADC1)
{
/*##-1- Reset peripherals ##################################################*/
__ADC1_FORCE_RESET();
__ADC1_RELEASE_RESET();
/*##-2- Disable peripherals and GPIO Clocks ################################*/
HAL_GPIO_DeInit(GPIOC, GPIO_PIN_3);
/*##-3- Disable the DMA Streams ############################################*/
HAL_DMA_DeInit(&hDMA2_ADC);
/*##-4- Disable the NVIC for DMA ###########################################*/
HAL_NVIC_DisableIRQ(DMA2_Stream0_IRQn);
}
if(hadc->Instance == ADC2)
{
/*##-1- Reset peripherals ##################################################*/
__ADC2_FORCE_RESET();
__ADC2_RELEASE_RESET();
}
if(hadc->Instance == ADC3)
{
/*##-1- Reset peripherals ##################################################*/
__ADC3_FORCE_RESET();
__ADC3_RELEASE_RESET();
/*##-2- Disable peripherals and GPIO Clocks ################################*/
HAL_GPIO_DeInit(GPIOF, GPIO_PIN_7);
} 
}

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Amel NASRI
ST Employee
Posted on August 04, 2015 at 15:24

Hi Keaven,

The following functions are not defined in the ADC HAL driver:

__ADC1_FORCE_RESET();

__ADC1_RELEASE_RESET();  __ADC2_FORCE_RESET();

__ADC2_RELEASE_RESET();  

__ADC3_FORCE_RESET();

__ADC3_RELEASE_RESET();

You need to call:

ADCxyz_FORCE_RESET();

ADCxyz_RELEASE_RESET();

Please note that current STM32CubeF4 package version is 1.7.0. For sure there are some enhancements made in version besides to the support of new F4 products.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

keaven
Associate II
Posted on August 04, 2015 at 16:47

Hi Mayla,

I validate the version and I am using 1.6.0 .  The reason that I am not up to date is simply I am getting the update from Keil uVision 5 package update.  It takes a bit longer to get the latest version.

In which header file do I find ADCxyz_FORCE_RESET() macros? I cannot find them.

Finally, the macros ADC1_FORCE_RESET() is present in stm32f4_hal_legacy.h.  Any reason why the build process cannot find them?

Thank  you for your help.

keaven
Associate II
Posted on August 04, 2015 at 17:04

Hello again,

I just noticed by looking at the STM32F4 reference manual ( RM0090) that the STM32F4 doesn't actually have seperate reset for ADC1, ADC2, or ADC3.  It has a common reset for the whole controller.

So I have to use the common reset .

Thank you again.

Amel NASRI
ST Employee
Posted on August 04, 2015 at 17:55

You are right Keaven, there are no functions calledADCxyz_FORCE_RESET & ADCxyz_RELEASE_RESET I referred to the ADC example in Cube package where these are labels only used there.

The correct ones are:

__ADC_FORCE_RESET();
__ADC_RELEASE_RESET();

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.