cancel
Showing results for 
Search instead for 
Did you mean: 

ADC_SoftwareStartConvCmd will enable external trigger?

chaos
Associate
Posted on November 17, 2011 at 10:13

Hi all,

I'm using StdPeriph lib and saw there is such code in 

stm32f10x_adc.c:

#define CR2_EXTTRIG_SWSTART_Set     ((uint32_t)0x00500000)

and 

/**

* @brief Enables or disables the selected ADC software start conversion .

* @param ADCx: where x can be 1, 2 or 3 to select the ADC peripheral.

* @param NewState: new state of the selected ADC software start conversion.

* This parameter can be: ENABLE or DISABLE.

* @retval None

*/

void ADC_SoftwareStartConvCmd(ADC_TypeDef* ADCx, FunctionalState NewState)

{

/* Check the parameters */

assert_param(IS_ADC_ALL_PERIPH(ADCx));

assert_param(IS_FUNCTIONAL_STATE(NewState));

if (NewState != DISABLE)

{

/* Enable the selected ADC conversion on external event and start the selected

ADC conversion */

ADCx->CR2 |= CR2_EXTTRIG_SWSTART_Set;

}

else

{

/* Disable the selected ADC conversion on external event and stop the selected

ADC conversion */

ADCx->CR2 &= CR2_EXTTRIG_SWSTART_Reset;

}

}

IIRC, set the bit 20 will enable the external trigger. So, why enable the external trigger when ADC_SoftwareStart ?

Thanks in advance.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0