2010-12-04 5:40 PM
adc noise
2011-05-17 5:17 AM
Hi,
I noticed that the configuration I did is working but the TxBuffer is getting filled very quick. The timer was used to control the speed that the TxBuffer was filled. Thanks2011-05-17 5:17 AM
I changed the topic because the old one is not appliable anymore and nobody answered
2011-05-17 5:17 AM
''Is it normal to listen to a background noise with my voice when using the internal ADC?''
The ADC is irrelevant - all electrical signals are subject to noise! And, of course, acoustic signals are also subject to noise! Minimising the noise requires very careful design of the recording environment, the microphone, and the analogue input circuitry. A major source of noise for an internal ADC specifically can be all the other digital circuits in the chip. There is a huge amount of material available in books, on the internet, etc, about low-noise design - including low-noise design specifically for ADC inputs...''I noticed that, even though when there is nothing in the input, the ADC stores something around 2048 (4096/2). Is it normal?'' You haven't given any details at all of your input circuitry to the ADC (or even what particular STM32 part you're using) - so it's impossible to say whether it is to be expected for your particular setup! But remember that an audio signal has both positive and negative excursions - so it would not be unusual to arrange for an ADC to give a ''half-scale'' output at zero...2011-05-17 5:17 AM
Hi Neil,
I'm using STM32F107VC in an IAR Development Kit. Does anyone know how the buzzer works? I'd like to use it in its maximum volume. Thanks2011-05-17 5:17 AM
According to the schematic, it's connected to PD.13 (TIM4_CH2)
http://www.iar.com/website1/50.0.1.0/489/IAR-STM32F107VC-SK_REV-1.pdf One might assume you drive it with the GPIO pin directly, or use TIM4 to PWM, or otherwise excite it. Try looking at the data sheet for the PB1221P and the schematic. http://www.mallory-sonalert.com/specifications/PB-1221P.pdf http://www.mallory-sonalert.com/specifications/PB-1221PQ.pdf Can't be that hard can it, to drive it with a 2.048 KHz square wave?2011-05-17 5:17 AM
Looks like the sounder is a self oscillating device. Just power it by driving the transistor ON. Since the sounder is rated for a 2.5V supply and is connected to a 3.3V supply it's already being overdriven.
2011-05-17 5:17 AM
Looks like the sounder is a self oscillating device. Just power it by driving the transistor ON.
No the specs suggest it needs a ~2 KHz square-wave IAR/Olimex example code looks to be banging it at about 2.5 KHz Slightly edited for clarity, but still overly verbose... TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; GPIO_InitTypeDef GPIO_InitStructure; TIM_OCInitTypeDef TIM_OCInitStructure; // Buzzer init // GPIO enable clock and release Reset RCC_APB2PeriphResetCmd( RCC_APB2Periph_GPIOD | RCC_APB2Periph_AFIO, DISABLE); RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOD | RCC_APB2Periph_AFIO, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOD, &GPIO_InitStructure); // Init PWM TIM4 // Enable Timer4 clock and release reset RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4,ENABLE); RCC_APB1PeriphResetCmd(RCC_APB1Periph_TIM4,DISABLE); TIM_InternalClockConfig(TIM4); GPIO_PinRemapConfig(GPIO_Remap_TIM4,ENABLE); // Time base configuration TIM_TimeBaseStructure.TIM_Prescaler = 110; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 0x100 - 1; // 8 bit resolution TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM4,&TIM_TimeBaseStructure); // Channel 2 Configuration in PWM mode TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_Pulse = 0x80; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset; TIM_OC2Init(TIM4,&TIM_OCInitStructure); // Double buffered TIM_ARRPreloadConfig(TIM4,ENABLE); // TIM4 counter enable TIM_Cmd(TIM4,ENABLE);
2011-05-17 5:17 AM
Thanks!
I concluded that isn't possible to increase the buzzer volume. It's made to achieve its maximum when oscillating at 2048Hz. In the directory below, there is very clear example about how to change the frequency of the Timer PWM Mode, used with Buzzer. \arm\examples\ST\STM32F10x\stm32f10x_stdperiph_lib\Project\STM32F10x_StdPeriph_Examples\TIM\PWM_Output Now I'm looking for a buzzer which has a good frequency response at the higher audible frequency possible. If you have any suggestions...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.