cancel
Showing results for 
Search instead for 
Did you mean: 

ADC audio sampling circuit

sv2agw
Associate II
Posted on May 13, 2015 at 16:36

Hi

I connected audio to ADC and can DSP with success only if the audio is from speaker out. I need to connect audio from a device which outputs 500mvpp. I am using the follow input circuit

http://www.frinos.com/adc.png

Thank you in advance for any help

Georges

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
raptorhal2
Lead
Posted on May 13, 2015 at 17:52

500 mv will give a swing of 1/6 the ADCs range of 4095 counts. But the capacitor, 2 resistors and the ADC input resistance and capacitance form a network that will change that. Put a 'scope on the ADC input signal to see if it is as expected.

Cheers, Hal