cancel
Showing results for 
Search instead for 
Did you mean: 

32H563Zi can't work in VDD=1.8V?

Charles63
Associate II

Hi, Sir:

 Currently using H563ZI (MB1404C) to develop programs.
When VDD=3.3V, MCU works normally
When VDD=1.8V, the MCU functions abnormally (USB function fail), but the specification indicates that it can support VDD=1.8V. Where should I set this on the EVK?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Jaroslav JANOS
ST Employee

Hello @Charles63,

what is the voltage on VDDUSB? Is it same as VDD? If yes, and you are using USB, it must be above 3.0V.

BR,
Jaroslav

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hi, Sir

 

H563ZI(MB1404C) EVB

  • VDD = 3.3V + VDD_USB = 3.3V --> USB function is normal
  • VDD = 1.8V + VDD_USB = 3.3V --> USB function abnormality
Charles63
Associate II

Hi, Sir :

   How to solve this problem? 

  • Issue --> VDD = 1.8V , VDDUSB = 3.3V , USB function is not work