12864B I2C LCD I will ask. (STM32F429)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-28 10:51 PM
Hi everyone
That link page 12864 I2C LCD(
)
I have a question. (STM32F207)12864 to STM32F207 and try to use it.There is only AVR or Arduino sample as below.I will find the LCD STM sample source.Could you change the AVR source below to ST HAL based?I did not think of AVR, so I did not have time.Have a nice day!!#include <avr/io.h>
#include <avr/interrupt.h>
#include <avr/signal.h>
void I2C_init(void)
{
TWBR = 0x80; // set the bit rate
TWAR = 0x00; // set the slave address
TWSR |= 0x00; // Set the division factor
TWCR = 0X00;
DDRC=DDRC&0XF7;//PC3 check LCD BUSY
PORTC=PORTC|0X08;
}
void busy(void)
{
while(PINC&0x08); //Check LCD busy
}
// Arbitration becomes host and sends START signal
// return value: 1 for success, 0 for failure
uint8_t I2C_start(void)
{
busy();
TWCR|=(1<<TWINT)|(1<<TWEN)|(1<<TWSTA);
while(!(TWCR & (1<<TWINT)));
if(((TWSR & 0xf8)!=0x08) && ((TWSR & 0xf8)!=0x10))
return 0;
return 1;
}
// stop communication and send STOP signal)`
void I2C_stop(void)
{
TWCR|=(1<<TWINT)|(1<<TWEN)|(1<<TWSTO);
}
// Issued from the machine address and write command, that is, SLA + W, into the MT mode
// return value: 1 for success, 0 for failure
uint8_t I2C_to_write(void)
{
TWDR=0;
TWCR=(TWCR&0X0F)|(1<<TWINT)|(1<<TWEN);
while(!(TWCR &(1<<TWINT)));
if((TWSR & 0xf8)!=0x18)
return 0;
return 1;
}
// send data to the slave
// return value: 0 for failure, 1 for ACK, 2 for NOT ACK
uint8_t I2C_send(uint8_t data)
{
busy();
TWDR=data;
TWCR=(TWCR&0X0F)|(1<<TWINT)|(1<<TWEN);
while(!(TWCR & (1<<TWINT)));
if((TWSR & 0xf8)==0x28)
return 1;
else if((TWSR & 0xf8)==0x30)
return 2;
return 0;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-11 10:54 AM
Have you tried setting up a project with CubeMX then using the HAL commands like 'HAL_I2C_Master_Transmit'? CubeMX is really simple and you can find tutorials on YouTube.