2021-08-31 5:42 AM
In Standby mode it is given like this....
(1.2 V domain powered off).
All 1.2 V domain clocks OFF
what does this means?
2021-08-31 8:29 AM
Hello @AR.7 ,
I think you are referencing to STM32F75xx family ? "1.2V domain clock" is the one you find under the datasheet supplying kernel logic (CPU,digital,RAM,..)
On STM32, you can achieve lower power consumption by switching off some domains but keeps some clocks such as RTC for example.
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.