2023-08-28 4:14 AM
Hi ,
I am using stm32wl55ccu 48 pin QFN MCU to drive a 3 phase brushless motor using 3-phase complementary PWM output signals using TIMER 1. I have seen at the datasheet that this 48 QFN package is missing the complementary output of TIMER1 ,Channel 3, TIM1_CH3N (which is present at the BGA version). Is it possible to generate the 3-rd phase complementary output PWM signal in another way ?(like using timer 2 in a master/slave configuration).
Thank you, Joe.
Solved! Go to Solution.
2023-09-07 6:30 AM
Hello YY55,
It is technically possible to synchronize TIM1(master) and TIM2(slave), examples are available in the reference manual of the chip (chapter 24.3.26 and 25.3.19):
But your firmware will have to take care about the deadtime insertion between the high side and low side on the third phase (which will be done automatically on phase 1 and 2 by TIM1 in your case).
Another solution could be to choose (if possible), a gate driver that needs only 3 PWM input signals ( like L6230: https://www.st.com/en/motor-drivers/l6230.html )
Best regards
2023-09-07 6:30 AM
Hello YY55,
It is technically possible to synchronize TIM1(master) and TIM2(slave), examples are available in the reference manual of the chip (chapter 24.3.26 and 25.3.19):
But your firmware will have to take care about the deadtime insertion between the high side and low side on the third phase (which will be done automatically on phase 1 and 2 by TIM1 in your case).
Another solution could be to choose (if possible), a gate driver that needs only 3 PWM input signals ( like L6230: https://www.st.com/en/motor-drivers/l6230.html )
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.