cancel
Showing results for 
Search instead for 
Did you mean: 

Why on STM32CUBEF1 code version 1.8.1 bit FLASH_ACR_PRFTBE is not define? while on previous version on 3.5.0 it was defined.

STiwa.1
Associate

STM32F1_3.5.0 has bit description of FLASH_ACR_PRFTBE0693W000003RYZQQA4.jpg

STM32CUBEF1_1.8.1 has no bit description of FLASH_ACR_PRFTBE0693W000003RYZGQA4.jpg

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

It's still "used" in stm32f1xx_hal_flash.h, so probably a bug if not defined:

https://github.com/STMicroelectronics/STM32CubeF1/blob/441b2cbdc25aa50437a59c4bffe22b88e78942c9/Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal_flash.h#L231

/**
  * @brief  Enable the FLASH prefetch buffer.
  * @retval None
  */ 
#define __HAL_FLASH_PREFETCH_BUFFER_ENABLE()    (FLASH->ACR |= FLASH_ACR_PRFTBE)
 
/**
  * @brief  Disable the FLASH prefetch buffer.
  * @retval None
  */
#define __HAL_FLASH_PREFETCH_BUFFER_DISABLE()   (FLASH->ACR &= (~FLASH_ACR_PRFTBE))

If you feel a post has answered your question, please click "Accept as Solution".

Thanks.

I read manual and got to know only flash half cycle access can be control rest bits are reserved.0693W000003Re0bQAC.jpg