cancel
Showing results for 
Search instead for 
Did you mean: 

Why is AXI RAM and RIF necessary when using DCMIPP?

pawatJoy
Associate III

Hello, i just wanna take a snapshot by STM32N6570-DK with IMX335. I am using SnapshotDecimation as my reference. after reviewing the code. i wonder why AXI RAM3/4 and RIF are necessary for this project i saw it in 'HAL_DCMIPP_MspInit' function, but i didnt found anything about AXI RAM in other parts of the code.

anyone can explain why does axiram necessary for this project?

void HAL_DCMIPP_MspInit(DCMIPP_HandleTypeDef* hdcmipp)
{
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
  RAMCFG_HandleTypeDef hramcfg  = {0};
  RIMC_MasterConfig_t RIMC_master = {0};
  if(hdcmipp->Instance==DCMIPP)
  {
    /* USER CODE BEGIN DCMIPP_MspInit 0 */
    /*** Enable peripheral clock ***/
    /* Enable DCMIPP clock */
    __HAL_RCC_DCMIPP_CLK_ENABLE();

    __HAL_RCC_DCMIPP_FORCE_RESET();
    __HAL_RCC_DCMIPP_RELEASE_RESET();

    /*** Configure the NVIC for DCMIPP ***/
    /* NVIC configuration for DCMIPP transfer complete interrupt */
    HAL_NVIC_SetPriority(DCMIPP_IRQn, 0x07, 0);
    HAL_NVIC_EnableIRQ(DCMIPP_IRQn);

    /*** Enable peripheral clock ***/
    /* Enable CSI clock */
    __HAL_RCC_CSI_CLK_ENABLE();

    __HAL_RCC_CSI_FORCE_RESET();
    __HAL_RCC_CSI_RELEASE_RESET();

    /*** Configure the NVIC for CSI ***/
    /* NVIC configuration for CSI transfer complete interrupt */
    HAL_NVIC_SetPriority(CSI_IRQn, 0x07, 0);
    HAL_NVIC_EnableIRQ(CSI_IRQn);

    /* USER CODE END DCMIPP_MspInit 0 */
    /* USER CODE BEGIN DCMIPP_MspInit 1 */

    /* DCMIPP Clock Config */
    /* DCMIPP clock configuration */
    /* Typical PCLK is 333 MHz so the PLL1 is configured to provide this clock */
    /* Configure DCMIPP clock to IC17 with PLL1  */
    /* PLL1_VCO Input = HSI_VALUE/PLLM = 64 Mhz / 4 = 16 */
    /* PLL1_VCO Output = PLL3_VCO Input * PLLN = 16 Mhz * 75 = 1200 */
    /* PLLLCDCLK = PLL3_VCO Output/(PLLP1 * PLLP2) = 1200/4 = 300Mhz */
    /* DCMIPP clock frequency = PLLLCDCLK = 300 Mhz */
    PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DCMIPP;
    PeriphClkInitStruct.DcmippClockSelection = RCC_DCMIPPCLKSOURCE_IC17;
    PeriphClkInitStruct.ICSelection[RCC_IC17].ClockSelection = RCC_ICCLKSOURCE_PLL1;
    PeriphClkInitStruct.ICSelection[RCC_IC17].ClockDivider = 4;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
    {
      Error_Handler();
    }

    PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_CSI;
    PeriphClkInitStruct.ICSelection[RCC_IC18].ClockSelection = RCC_ICCLKSOURCE_PLL1;
    PeriphClkInitStruct.ICSelection[RCC_IC18].ClockDivider = 60;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
    {
      Error_Handler();
    }

    /* IMX335 Sensor HW Reset */
    /* Enable GPIO clocks */
    __HAL_RCC_GPIOC_CLK_ENABLE();
    __HAL_RCC_GPIOD_CLK_ENABLE();

    GPIO_InitTypeDef gpio_init_structure = {0};

    /* Initialize camera NRST pin */
    gpio_init_structure.Pin       = GPIO_PIN_8;
    gpio_init_structure.Pull      = GPIO_NOPULL;
    gpio_init_structure.Mode      = GPIO_MODE_OUTPUT_PP;
    gpio_init_structure.Speed     = GPIO_SPEED_FREQ_VERY_HIGH;
    HAL_GPIO_Init(GPIOC, &gpio_init_structure);

    /* Initialize camera EN pin */
    gpio_init_structure.Pin       = GPIO_PIN_2;
    gpio_init_structure.Pull      = GPIO_NOPULL;
    gpio_init_structure.Mode      = GPIO_MODE_OUTPUT_PP;
    gpio_init_structure.Speed     = GPIO_SPEED_FREQ_VERY_HIGH;
    HAL_GPIO_Init(GPIOD, &gpio_init_structure);

    /* Camera sensor Power-On sequence */
    /* Assert the camera Enable and NRST pins */
    HAL_GPIO_WritePin(GPIOC, GPIO_PIN_8, GPIO_PIN_SET);
    HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_RESET);
    HAL_Delay(200);   /* NRST and Enable signals asserted during 200ms */

    /* De-assert the camera STANDBY pin (active high) */
    HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_SET);
    HAL_Delay(3);     /* NRST de-asserted during 3ms */

    /* SRAM3 and SRAM4 memories clock enable */
    LL_MEM_EnableClock(LL_MEM_AXISRAM3);
    LL_MEM_EnableClock(LL_MEM_AXISRAM4);

    /* Power On AXSRAM3 and AXISRAM4 */
    hramcfg.Instance = RAMCFG_SRAM3_AXI;
    HAL_RAMCFG_EnableAXISRAM(&hramcfg);

    hramcfg.Instance = RAMCFG_SRAM4_AXI;
    HAL_RAMCFG_EnableAXISRAM(&hramcfg);

    __HAL_RCC_RIFSC_CLK_ENABLE();

    RIMC_master.MasterCID = RIF_CID_1;
    RIMC_master.SecPriv = RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV;

    HAL_RIF_RIMC_ConfigMasterAttributes(RIF_MASTER_INDEX_DCMIPP, &RIMC_master);
    HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_DCMIPP , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV);
    /* USER CODE END DCMIPP_MspInit 1 */
  }

}

 

1 ACCEPTED SOLUTION

Accepted Solutions
Ch_JE
ST Employee

Hello ,

the AXI SRAM3 and 4 are used as camera frame buffer #define BUFFER_ADDRESS 0x34200000 

Ch_JE_0-1770993428659.png

For the RIF part: DCMIPP is a bus master and therefore needs its RIF master and slave attributes to be configured; otherwise, its transfers to RAM will be blocked. Configure the master attributes to authorize DCMIPP’s memory accesses, and configure the slave attributes to authorize CPU access to DCMIPP registers.

Best Regards,

View solution in original post

1 REPLY 1
Ch_JE
ST Employee

Hello ,

the AXI SRAM3 and 4 are used as camera frame buffer #define BUFFER_ADDRESS 0x34200000 

Ch_JE_0-1770993428659.png

For the RIF part: DCMIPP is a bus master and therefore needs its RIF master and slave attributes to be configured; otherwise, its transfers to RAM will be blocked. Configure the master attributes to authorize DCMIPP’s memory accesses, and configure the slave attributes to authorize CPU access to DCMIPP registers.

Best Regards,