When configuring STM32F107RC FreeRTOS, the interrupt CALLBACK function is not called
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-09-10 11:14 PM
Hello.
I have some questions while testing a product using the 107MCU.
As the title suggests, when I set up FreeRTOS and create a task, the commonly used callback functions cannot be called:
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
If I remove the task creation function, it operates normally.
Do you know why this is happening?
Thank you.
Labels:
- Labels:
-
FreeRTOS
0 REPLIES 0