USB performance on STM32H7
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-03-25 9:15 AM
Hi All,
This is related to performance on USB Host in FS mode. I have built custom board with STM32H743BIT6.Main interfaces on this are - USB FS Host, SD Card (SDeMMC interface used), LTDC, 16Mbyte SDRAM and Ethernet. All the interfaces are up and running except Ethernet. Need to debug further on this one as I could see that the phy communication itself didn't succeed.
I have created the project using cubeMX.USB is running on internal 48RCsystem is working at 400MHz sourced by external crystal oscillator 25MHz.
USB host mode + SD+LTDC+Fat FS + FREERTOS - is up an druning.
However the read performance measured on USB is at around 600kbits per second. SD performance after IP internal DMA enabled and running at 25Mhz I get close to 5.7MByytes per second.
Any possibility to improve the host performace ? I have tried enabling IP internal DMA still performance remained same.Can someone in this forum please help improve performance ?
- Labels:
-
STM32H7 series
-
USB