cancel
Showing results for 
Search instead for 
Did you mean: 

USB Nucleo-144

wh
Associate III
Posted on October 13, 2016 at 14:28

I'm trying to use the USB device of the STM32F429 mounted on a NUCLEO-144 evaluation kit.  I enabled the USB controller using the STM32CubeMx tool and created a Atollic true studio project. The USB controller is configured in CDC mode. building and running the program on the kit works OK but when I connect the kit to a windows machine I get the  Windows message ''Unknown USB device (Invalid Device Description). I did install the latest Virtual COM device driver (downloaded the VCP_V1.4.0_Setup.exe).  The .inf VID PID match the settings in the generated code.

Did anyone experience the same problem?

Does anyone know a solution? Is it the generated code that is wrong or do I don't have the correct virtual com driver for Window 10?

Thanks Wim

#usb-nucleo-144-stm32f429zi
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on October 31, 2016 at 14:35

Hi Wim,

•Could you please precise witch CUBEMX version are you using? If you are using an old version, I recommend you to use the last version 4.17

•If the issue persist again please share you .ioc file for check

-Syrine-